ACTION#.TASKID

Description

Some tasks require a task ID to specify what is acted upon. For example, if setting the value of DOUT2 from the source, then ACTION#.TASK = 1 (set Digital Output from Source), and ACTION#.TASKID = 2.

ACTION#.TASK must be set before ACTION#.TASKID. If ACTION#.TASK is modified, then the range and units of ACTION#.TASKID may be modified, and the value will be defaulted.

Not all tasks require a task ID.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

Depends on ACTION#.TASK

Default Value

Depends on ACTION#.TASK

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported